Other Parts Discussed in Thread: ADS131M08, ADS7038
Tool/software:
Hi everyone,
In my project, TLV2548 combined with Roche coil is used for AC three-phase current acquisition, and there are two questions about this chip, which are as follows:
1、Are the parameters of TLV2548IPW and TLV2548IDW the same except for different package?
2、Does TLV2548 have functions related to calibration of three-phase electricity? Such as phase calibration.
3、3.3V is used as the power supply of the chip. If SCLK is used as the conversion clock source, is the maximum conversion rate 6MHz? At the maximum conversion rate, is the maximum operating current still the nominal value of 1.6mA?
Thanks and regards,
Ivy