Part Number: DAC38J84
Tool/software:
In the DAC38J84 specification, it is mentioned that only JESD204B subclass 1 is supported. Since the SYNCb signal is exclusively used by subclass 2, does this mean that this signal and all related configurations are currently unused?
Additionally, in config72, bits 3:1 allow selecting the JESD204B subclass, but as i mentioned, the documentation states that only subclass 1 is supported. Does this imply that the DAC38J84 was initially designed to support all three JESD204B subclasses, but at some point, this was discontinued? For instance, were signals like SYNCb (used by subclass 2) left with no functionality in the final implementation?
I find this a bit confusing and would appreciate clarification.