Tool/software:
Hello,
I am using dual supply operation of TPL0102. Can I use it like this, as given at the below scheme? I need to get -2V to 0V from Wa and Wb.
Regards,
Eren Yildiz

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
I am using dual supply operation of TPL0102. Can I use it like this, as given at the below scheme? I need to get -2V to 0V from Wa and Wb.
Regards,
Eren Yildiz

Hi Eren,
The device will act as a voltage divider with the wiper output ranging from HA to LA. You will not get the full 8-bits of resolution because you are not using the full range, but yes, you can use the device as shown in your circuit. Make sure your I2C controller will work with 2.5V logic.
Best,
Katlynne Jones