Hi.
I am looking for a fast DAC converter (>1Gsps) for my FPGA based communication system design.Unfortunately after I got the DAC3484EVM, I found this might not fit my application.
If I am correct, the DAC3484 has a maximum sample rate of 1.25 Gsps at the digital input end. But for each of the 4 output channel DAC, the sampled digital input actually has a maximum rate of 1.25G/4=312.5Msps. Is this correct?
In my case. I only need one channel and the signal generated from the FPGA has an minimum sampling rate of 800MHz, which mean I will need an 800Msps DAC. Could you suggest which module I should look at? I found DAC5681, would that suit?
And just a bit of interest, for the multichannel DAC chips you have, the DAC module for each channel actually has a sampling rate of 1/n of the input sampling rate (n channels). is that correct?