Tool/software:
I wish to use the ADS8028 to interface external signals on the analog side, with a xilinx FPGA connected to the digital side.
Due to the FPGA Power-On/Off Power Supply Sequencing, I want provide immediately AVDD (5V), and, only later, i will provide DVDD, 3,3V (at the end of FPGA power-on sequence) 
I need to know if the ADS8028 can work in this way, or, if problems can arise in the short period in which power supply is provided only on AVDD pin.
thank you in advance for your help.
best reguard