Other Parts Discussed in Thread: ADS127L18
Tool/software:
Hello,
We recently purchased the ADS127L18EVM-PDK evaluation board and have been using the ADS127L18EVM-PDK-GUI to collect some data for our experiment.
I gave the following settings in the GUI to capture data at a lower rate.
Filter: Wideband filter
Clock: 3.2MHz and OSR: 4096, this gave me the data rate as 390.6 Hz.
My application demands a larger set of data to be captured. To test, I provided 1,000,000 samples under the Samples control field in the GUI, theoretically, it should have run for 42 mins but the adc ran just for 4 mins and stopped. However, the data log did consist of 1 million samples.
I also tried giving 40000 samples to capture, but instead of running for 100 seconds, it just ran for 10 seconds and stopped.
Would it be possible to explain the behavior here? Because I am a bit surprised here.
I should be able to run the ADC for at least 20 mins to capture the data that I am experimenting with and my data rate ranges from 5000 Hz to 300 Hz.
Looking for some help here.
Regards,
Shan