Other Parts Discussed in Thread: AMC1306M05
Tool/software:
hi
I want to know the DC accuracy parameter from -250mV to -320mV and 250mV to 320mV for a worst Case Calculation, could you provid it? thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
hi
I want to know the DC accuracy parameter from -250mV to -320mV and 250mV to 320mV for a worst Case Calculation, could you provid it? thank you!
Hello,
The region between the FSR of the device and the clipping voltage will have reduced accuracy compared to staying within the recommended operating conditions but should be similar. This is not something we have specified in the data sheet. What is your system's accuracy requirements?
Best regards,
Eva
We cannot guarantee performance past the FSR since it is outside of the recommended operating conditions and is not specked. If you plan on measuring within the clipping range, I would recommend adjusting your shunt resistor size to get the input within the acceptable range to ensure you meet your accuracy requirements. What's you application? What is your current sensing range?
Best regards,
Eva
What's you application?---------- PMSM MOTOR phase Current sample
What is your current sensing range? -----shunt resistor value is 4mΩ, Motor peak current is 77.48A, AMC1306M25 input max 77.48*4.01=313.1mV(shunt resistor accuracy 1%),Consider the the ADC accuracy, I dont want to see it beyonds 320mV
I would recommend sizing the shunt resistor such that the input to the AMC device is not beyond 250mV. A 3mΩ-3.2mΩ would work well. Be sure to consider power dissipation as well when selecting a shunt resistor.
Also, for higher currents such as 77A, you could also consider the AMC1306M05. This has a 50mV input and is typically used for higher currents.
Best regards,
Eva