This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5687 Power Up Sequence

Other Parts Discussed in Thread: DAC5687

In looking at the datasheet for the DAC5687, it says in the "Absolut Maximum Ratings" section that AVDD (3.3V) should never be more that 2.6V above DVDD (1.8V) or 0.5V less than.

But in the "Power-Up Sequence", it states that DVDD should be powered up first. If this occures, then AVDD will be 1.8V less than DVDD, which seems like it breaks the Absolute Maximum Rating rule.

Am I reading this correctly? And if so, should the Power-Up Sequence be followed or is this potentially harmful?

 

Thanks!

-Brian