Tool/software:
Dear TI Forum,
We have a DAC39RF10EVM evaluation board with FMC and FMC+ connectors, and we need to perform frequency output testing from the DAC using NCO and DDS, verifying the output on DCA0.
Could you please provide the user manual for this board and clarify the following points?
- Input Signals:
- What are the required input signals for LMX and LMK on this board?
- What is the recommended frequency input for these signals?
- GUI Usage:
- How do we configure and use the GUI to control the DAC settings using NCO and DDS?
- Xilinx Evaluation Board Compatibility:
- Which Xilinx evaluation board is suitable for interfacing with the DAC39RF10EVM to test JESD204?
- Can we use TI’s JESD IP for this board? If yes, please provide guidance on bringing it up using USB or SPI.
- Reference Design:
- If available, could you share a reference design or direct us to a High-Speed Data Converters Applications Engineer for further assistance?
This information will greatly help us in setting up and testing the board efficiently. Looking forward to your support.
Best regards,
Balu