Part Number: TI-JESD204-IP
Other Parts Discussed in Thread: ADS52J90
Tool/software:
I have explored the TI-JESD IP in loop back mode where SYSREF from TX looped back to RX and continues to run.
In our prototype board, we are using LMK0426 and ADS52J90 for clock generation and data acquisition where we see that the JESD is locking and continues to receive the data.
But we see that the SYSREF discontinues in around 1.2 ms while the data is still being received with valid data on JESD.
LMK0426 has been set in "SYSREF Request mode" which basically looks for SYNC signal. (I am using SYNC inverted from SYNC~ from TI JESD IP).
We intend to use SYNC as two ADCs to be connected to same JESD IP. My question is whether this discontinuation of SYSREF is ok and expected behavior.

Every time JESD is reset and starts, we see above behavior.
Hope to hear soon.
Thanks & regards,
Trushal