Part Number: DAC80502
Other Parts Discussed in Thread: DAC60508, DAC80508, DAC81402, DAC61402
Tool/software:
Hi TIer
My customer want us this chip for medical high voltage control.
For RSTSEL pin , we see the describe in datasheet.
How do I change the RSTSEL voltage while the DAC is outputting voltage(working), will I make the DAC output to 0V?
Also, what are the restrictions on the use of the RSTSEL pin function? When VDD is greater than 5V, how is it controlled?
Finally, if VDD=5.5V, can the SPI communicate using 5.5V logic or 3.3V logic?
Do we have a higher price/performance chip, more performance than the DAC80502, we have an ADI competitor ad5689, they have good performance, But a little more expensive .
Thank you very much.