Other Parts Discussed in Thread: ADS52J90
Tool/software:
Hi,
I have set RX K Value as 4 in TI_JESDC IP, as per previous thread.
With the ADC connected and JESD locked, LMFC pulses every 3rd clock but as set value 4 above, we expect LMFC pulse every 4rth clock cycle.
It may be due the the default setting in ADS52J90 (Number of frames per multiframe K =3).
We tried to change the value of K with "force K Value" and "K value" in registers 0x49 and 0x53 respectively but still getting LMFC pulsing every third cycle.
We are operating ADC in 32 channel mode, 4 lane mode, hence having even number for K value is important to distinguish between even and odd ADC samples.
Please let me know if I am missing anything here.

Also please note that rx_sysref_realign count reaching max "f" and may be increasing further as I can see stretching in between in rx_sysref

Thanks,
Trushal