Other Parts Discussed in Thread: DAC8718, DAC7718EVM
Hello,
I have a board with a DAC7718, used in bipolar mode (±12V). Other settings: WAKEUP, RST, LDAC, RSTSEL and USB/BTC are pulled-up. Vref is 2,5V, gain is set to 4x, no correction engine.
I can successfully communicate with the device (write-only, I don't have SDO routed) and I can update the DAC output.
The problem is the voltage range is between 0 and 10V, instead of -5 and 5V. In fact, the offset outputs voltage is 0V instead of 1.67V as stated in the datasheet (table 6, pag. 39).
Writing to the offset registers changes nothing, that is the offset output voltages are always 0V.
Did anyone run into this issue?
Thanks
Marco