This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S102: SPI interface not returning the expected data

Part Number: ADC128S102

Tool/software:

Hello

I am working with an ADC128S102 and a SAMRH71 microcontroller. I have been trying to read all 8 channels in sequence with SPI.

I have measured the SPI lines with an Oszilloscope to verify the way I am addressing the channels.

To me 3 signals (that are driven by the microcontroller) look exactly as I would expect them to (see figures below).

My issue now is, that the data that is returned to me on MISO does not represent the value I am measuring on the actual channel input of the ADC. For example, on channel 7 i have 0V but the adc returns a value bigger than 4000. In another case, i have varied the voltage on the input of channel 5 from 0.5V to 2V and the adc always returns a value close to 4000 as well.

I have also tried SCLK frequencies 250kHz, 1MHz, 8MHz, 10MHz, nothing seems to change.

All channels seem to return roughly the same value (between 3075 and 4025). The values that the individual channels return stay the same (+/- 1), but each channel has a little bit a different value (i.e. one always returns 3075/3075, another one always returns 4022/4023). I mention this, because at first I thought it looked like I was always getting the data of the same channel and therefore the addressing would be wrong, but this fact disproofes that theory in my opinion).

So i guess my question is, what could be a possible reason for the adc to not measure the right value or to not provide the expected data over the spi interface?

yellow: MISO

blue: SCLK

pink: MOSI

green: CS

Maybe someone has an idea what could be the issue here, I don't know what else to try or look at.

Thank you in advance!

Best regards

Tanja Regez

  • Hi Tanja,

    My first suspicion is that you aren't switching between channels correctly. ADD[2:0] bits are read by the ADC on the 3rd, 4th, and 5th rising edges, but in the first picture sent, it seems like there is a pulse on the 6th rising edge after CS falls.

    From your scope captures, it's a little hard to keep track of where one conversion ends and the other begins, but I would first double check that you are setting the ADD[2:0] bits correctly. One thing you can try is grounding CH0, and bringing CH1 to AVDD, and checking to see whether you can switch between the two reliably. For debug purposes, you might try sending only 16 SCLKs at a time between CS going high.

    Regards,
    Joel