This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC61404: power supply for dac41404

Part Number: DAC61404

Tool/software:

AVDD = +12V, AVSS = -5V, DVDD = +5V, IOVDD = +3.3V

Question:

1) if output short to +20V, can this device protected? (+20V is higher than AVDD, but lower than 40V limit)

2) If I need to set output = 0V to 10V, can it works?  The output is refer to AGND, not AVSS, right?

3) Does it require symmetric power supply for AVDD/AVSS?