Part Number: ADS1220
Tool/software:
Hello All,
I a heating related project we are using an ADS1220. The configuration is as following:
- 3-wire RTD
- conf0: 00h
- conf1: 00h
- conf2: 23h
-conf3: 70h
The ADC return only 0xFFFFFFFFFF after a read data command and changing the temperature on the RTD doesn't change anything.
I measure 0,983V over the 4,99KΩ Rref while over the PT100 I measure 0,011V.
Any idea what I'm doing wrong here?
Thanks for putting me on the right track.