This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW14J50EVM:DAC chip and evaluation board provided file of DAC38RF82(TSW14J50)

Part Number: TSW14J50EVM


Tool/software:

Is there any way to evaluate the higher output when I saw a DA output of 384 MHz in the example of using a separate clock from the TSW14J50 board and PLL on the DAC evaluation board?
And I would like to ask if two methods can be used to connect the output to the spectrum analyzer and check the FFT with GUI, and if there is a frequency limit for UI output.