Part Number: ADS1018-Q1
Other Parts Discussed in Thread: ADS1018
Tool/software:
Hi team,
Ads1018 debugging encountered the following problems:
Background: spi transmission mode: single 8bits, send twice/four times
Test process: Call API: adcStartup, reply 0x058B, check the chip manual and there is no problem.
Call API: readData, request to start a conversion, but the data returned by spi indicates that the SS bit is not set, and the E768 is powered by 1.3v, but no voltage is collected.
Is there a problem with the API call?
BR,
Ethan