This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP90100: SPI Data Read issue, LSB not reading correctly, even after using chip select between the two transactions

Part Number: LMP90100


Tool/software:

The problem I am having is exactly the one reported in this thread.

However the marked solution has not resolved the problem. I am still missing the the LSB, and the nature of that issue is no different if I use CS between the two transaction of a read or none. The original example code for MSP430 in snac029.zip also does not assert CS between the two transactions either. 

The waveform for 0x13 is actually falling at the same time that SCK is rising. 

Are there any other possible solutions I could try?