Part Number: ADS7830
Tool/software:
Hi,
I have an ADS730 with Vdd at 5.2V and a Vref of 5.0V (from an LP2980-5.0 to ensure stability).
I have my ADC input on CH1 and COM connected to Gnd for single ended input. The remaining ADC channels are also connected to inputs (so not floating).
I expected to read values from 0 to 255 for input voltages from 0 to 255 over the range from 0 to 5.0V but the ADC is returning the maximum 255 at 4.19V, well below the 5.0V of Vref.
I have set the reading with PD0 and PD1 set to 1 for Internal reference on and A/D converter on and I do not change these values.
I don´t understand why I am not getting the full range for the input.
Can anyone suggest what is wrong?
Thanks,
Nigel