Tool/software:
We are following instructions in the document SLAU833a.pdf for the evaluation of ADC12DJ3200-sp part with the Alpha Data FPGA board. There are couple things unclear in the instructions. On page 12 it says "The FPGA firmware is using unsigned data and K value of 4." The GUI shows K value of 3 and K-1 value of 3. Should I change the K value to 4? Why is K-1 value always set equal to K value by the underlying software?
On the directions on page 24 it says Launch ILA Analyzer. When we do this step a cryptic error message comes up. If select continue other cryptic error messages come up.
Please help.
The FMC+ EEPROM installed on the ADC12DJ3200EVMCVAL does not follow the Vita specification (64K instead of 2K) and is impossible to program. The footprint does not allow the correct EEPROM to be installed.
Please help.