Part Number: ADS9218
Tool/software:
Hello,
We've implemented the ADS9218 on a new design and the device is working nominally except that the current draw per device is 56mA when sampling at 10MSps instead of the datasheet's maximum rating of 40mA. Is this errata with the datasheet? How was the circuit implemented when those current ratings were determined?
Thanks,
Tighe