This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS124S08EVM: Specs of R_REF R68 Resistor and precision R_REF

Part Number: ADS124S08EVM

Tool/software:

Hello,

tl;Dr:

  • Is R68 a precise resistor?
  • Do resistors like R68 have a negative or positive temp coefficient in general?

I am currently investigating the Evaluation-Board and using your pt-100 highside 4 wire setup for measuring. I am fairly new to hardware development and have some questions about the R_REF of the EVAL board.

In your basic guide for RTD Measurement, you state a more precise R_REF leads to a better measurement, because the error of drift gets minimized. (Assuming the system gets calibrated to a known temperature(removing the initial accuracy error)). 

Is R68 considered precise?

I looked into the specs of the R68:

From the datasheet I got

  • 1 k Ohm
  • 0.1% Tol
  • 25 ppm/C

Are these specs correct?

Is 25 ppm/C considered low drift? There are resistors available with lower ppm.

The first measurements show a drift. The measurement environment is not regulated, so I am not sure if this is due to temperature changes. But I observed a neg. voltage-drift when the room heated up (In the morning when I start the heater in the office) and a positive voltage drift when the room gets colder. 

When the resistor has a pos. coefficient this would mean V_REF rises and the measured Voltage would drop(Lower codes). This would correlate to my observation.

Is this correct?

Measurement Settings:

  • Global chop enabled
  • SPS 5
  • sinc 3 filter enabled
  • 100 Ohm resistor to simulate 0 C(maybe also a drift source)

Thank you for your time Slight smile

Regards

Johanes

  • Hi Johannes Maier,

    The specific device used for R68 can be found in the Bill of Materials (Table 15). This is considered a precision resistor, but of course more precise resistors can be used (0.01%, 2ppm/C, etc.). This depends on the overall accuracy requirements of your system

    The resistor gain drift can be either positive or negative. I am not sure if you can predict a resistors drift without measuring it, as the drift depends on variations in the materials used to create the resistor as well as the manufacturing process. You should reach out to a resistor manufacturer e.g. Vishay, if you want more information

    -Bryan

  • Hello Bryan,

    thank you for your answer.

    Regards

    Johannes