Part Number: DAC63004
Tool/software:
Hi team..
I need to generate 5V and 0V voltage from DAC through SPI interface. I have tested DAC63004-EVM board with the given GUI, everything is working correctly.
Now I have to use custom board having DAC63004 in it through SPI. As I wanted to use same GUI which is provided for Eval board, I have removed R13, R14, R15, R16, R17, R18, R19, R20 resistors from eval board and through J1.1, J1.2, J1.3 and J2.2 I have taken SPI lines and given to my custom board. I am assuming these changes should work out for my requirement but it is not. I have checked that all signals are reaching my custom board at DAC63004 IC pin (SYNC, SCLK, and SDI) but not getting any output from custom DAC63004. Am I misssing out something.
Note: Output load condition in both the boards: Unloaded. GNDs are made common between eval board and custom board.
Regards
Chavan