Tool/software:
Just want to use below example,
1) connect GPI to MCU IO, pin, send 1KHz PWM
2) setup proper Rset, so can I generate constant current source for LED?
I mean, 1 KHz, 10mA low , 20mA high PWM
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Just want to use below example,
1) connect GPI to MCU IO, pin, send 1KHz PWM
2) setup proper Rset, so can I generate constant current source for LED?
I mean, 1 KHz, 10mA low , 20mA high PWM
Hi Liping,
The device will not send a PWM with this setup. This is meant for a constant current. You can set the DAC output to 1V or 2V with a 100ohm RSET to get 10mA and 20mA.
Best,
Katlynne Jones