Part Number: DAC39RF10EVM
Tool/software:
Dear TI team,
I am reaching out to inquire about the TI204C-IP. I am planning to connect the DAC39RF10EVM to the VCU118 using 64b66b JMODE10, outputting 2-channel 12-bit data to the DAC over 16 lanes. The data sampling rate is 5Gsps.
Using the transceiver wizard, I generated two 8-lane cores. I assigned the following lanes:
- Core 1: X0Y4, Y5, Y8, Y9, Y10, Y11, Y12, Y13
- Core 2: X0Y14, Y15, Y24, Y25, Y28, Y29, Y30, Y31
Could you confirm if this configuration is correct? Also, the clock is divided into two systems: Bank120, 121, 122, and Bank125, 126 from different SLRs. However, Bank122 is shared between Core 1 and Core 2. Would this cause any issues?
Since the DAC39RF10EVM can be connected to the TSW14J59 board under these conditions, I would appreciate it if you could explain how they are actually connected and operating.
Additionally, based on the reference design, I attempted to implement only Core 1 with 8 lanes under the above settings. However, after de-asserting tx_sync_reset following master_reset_n, tx_lane_data_ready does not assert, and data transfer does not start.
Furthermore, when I set NUMBER_OF_REFCLK_BUFFERS to 1 and Number_OF_QUADS to 3, qpll1_locked only returns 1.
Could you provide guidance on these issues?
I appreciate your support and look forward to your response.
Best regards,
tabe