Tool/software:
Hello,
I am interested in using a single REF5040 reference for 4 separate ADS8681 ADCs simultaneously sampling.
According to the schematic for the evaluation module, there is a jumper from the external reference to the REFIO pin of the ADC and the instructions state that the jumper should only be connected after the ADS8681 is programmed to turn off the internal reference.
Will I damage the ADS8681 in any way if I just directly connect multiple REFIO pins together and drive it with a single external reference? I imagine it will be no problem since the potential difference will probably be in the millivolts at most but I'd like to double check.
Thanks for the help.