This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DL3200EVM: ADC Control Package Read Register Issues

Part Number: ADC12DL3200EVM
Other Parts Discussed in Thread: ADC12DL3200, DAC12DL3200EVM

Tool/software:

Hello,

I have been using the control package provided through this post. I am having issues with the read register function since some registers such as the CHIP_TYPE Register at address 0x003 on the ADC12DL3200 are not returning their expected values on reset or power cycle, (in this case it should return 0x3 instead the read register function returns 0x0). There are many registers that have the same issue where a non-zero value should be returned but 0x0 is always returned. 

I appreciate any assistance or advice that can be provided.

Thanks,

Hunter