Part Number: ADC3422
Other Parts Discussed in Thread: ADC3442,
Tool/software:
Hello,
as in previous posts, I'm trying to validate the operation of the ADC using internally generated patters and test values.
I was able to receive correct data with "ramp" test (increasing numbers from 0 to 4095),
though the same number is repeated for four samples, i.e. as if the counter was 14bit wide,
and only bits [13:2] was produced at output.
Is it correct?
I'm NOT able yet to reproduce received data with the LFSR formula reported on previous answer.
I tested any possible bit offsets, trying to obtain a 12bit output from the 23bit shift register.
I'm using independent PRBS structures to check data from each independent channel.
No success so far...
Maybe a LFSR with length other than 23bit, or a different polynome is used?
Please let me know, or send me a sequence of values (and explain how they are obtained),
so I can what what is wrong...
I really need this test!
Thanks
Andrea