Part Number: ADS1292R
Other Parts Discussed in Thread: CC2340R5,
Tool/software:
Hello,
I am working on an ECG project which implements the ADS1292R in combination with the CC2340R5.
The ADS1292R does not react to any command.
Below is an example where I send a command to read the register CONFIG2

I appreciate any hint or advice
PS: I did check if the right pins are bond and the currents (AVDD=3V, DVDD=1.8)
Best regards
Mo K