This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1294R: Pace detection in ADS1294R using hardware approach

Part Number: ADS1294R

Tool/software:

Hi,

This is the circuit, we have implemented in our custom design to detect the pace detection in reference to the application note 

https://www.ti.com/lit/ug/slau511/slau511.pdf?ts=1743137551222&ref_url=https%253A%252F%252Fwww.google.com%252F

This does not seem to work.(Output at PACE_ALERT_OUT is zero always ) We use Whaleteq SECG 4.0 simulator to give pace inputs.

1) Do we have to make any changes in the circuit, not as per the application note?

2) Or Is this the correct way of evaluating?