This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS52J65: ADS52J65 ADC can't be arranged in sequence.

Part Number: ADS52J65

Tool/software:

Hi

We have designed a PCB that includes only a single ADS52J65 ADC. After loading the XC7Z045 FPGA with ADS52J65 firmware, the JESD204B are looking good.

I want to configure the platform to work with this setup, using 1 lane for data capture from the single ADS52J65 ADC.

After ADS52J65 is configured with ADS52J65_JESD_1L_160X_80_12.8Gbps(JESD 1-Lane mode),the D1,D2,D3,D4,D5~D8 lanes on ADS53J65 are turned on.

But the FPGA can't be arranged the 8-channel ADC in sequence.

I can reproduce the above-mentioned phenomenon, with to reconfigure or power cycle the system.

Could you provide guidance on how to modify configurations to ensure 8-channel D1~D8 linkup in sequence operation.

Thank you

Eddie