This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1292R: Issue with data retriaval

Part Number: ADS1292R

Tool/software:

Hello,

I am currently working on capturing data in continuous data mode using the ADS1292R. The device is configured to generate test signals (CONFIG2 = 0xA3). However, the ADS1292R repeatedly outputs the same value (0xC0 0x00 0x00) in each transmission cycle.

I have checked the register configurations and the current levels, and everything seems to be in accordance with the specifications.

Could anyone provide insight or suggestions to solve this issue?

Thank you in advance for your support.

Best regards,

Mo K