Tool/software:
When inputting a sine wave from 5MHz to 10MHz into the input of the AFE5808a and capturing ADC data, a 6dB attenuation is observed in the 10MHz ADC data compared to the 5MHz.
I am inquiring if there might be any setting issues that could be causing this problem. The sampling frequency being used is 40MHz.
There are no HPF (High-Pass Filter) components in the circuit that would cause such attenuation.