This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: ADS1298 - No DRDY or CLK signal after power-up

Part Number: ADS1298


Tool/software:

Hello,

I am working on a custom breakout board using the ADS1298, and I am facing an issue at startup. When I power the board with ±5V and set CLKSEL HIGH as well as START HIGH, I expect to see a signal on CLK or DRDY, but I observe nothing. It seems like the chip is completely inactive.

I have attached my schematic for reference.

Here are the key points I have checked:

  • Power supply is correct (+5V and -5V properly present on VCAP1, AVDD, and AVSS)

  • START is HIGH

  • CLKSEL is HIGH (so I assume the internal oscillator should be enabled)

  • MOSI, MISO, SCLK, and CS are not connected yet (testing without SPI for now)

I was expecting at least some activity on DRDY or SCLK, but all pins remain inactive.
Do you have any idea what could be wrong? Did I miss a critical initialization step?

Thanks in advance for your help!