This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI configuration to 16bit

Part Number: ADS131M08
Other Parts Discussed in Thread: TMS320F28379D

Tool/software:

Hello,
I have a question regarding the SPI configuration of the ADS131M08.
I´m using a TMS320F28379D DSP and I want to switch the word size of the SPI to 16 bit. I guess something went wrong in my configuration. The spi of the DSP is configured to 16 bit size (the maximum word size of the DSP). I send always ten words of 16 bit to the ADS131M08. You can see on

C1: Chip select
C2: Clock (10MBit)
C3: Dout (from DSP to ADS)
C4: Din (from ADS to DSP)

First of all I have read the status register. The result is 0x05ff (first word of the second frame is the response from the ADS) and this is ok.



Then I read the mode register. The result is 0x0510, this is also ok.




In the next step I want to change the word size to 16bit. For this I write the mode register with 0x0410, in order to change the bits WLENGTH[1:0] to 0:0.


When I read back the mode register, now I got a value of 0x1000. This is unexpected and not correct.




What is the problem in this configuation?


Thank you very much

Ralf