Part Number: TXB0108
Tool/software:
Hi Team,
We are using TXB0108 in our design. We have connected open drain pin in this level translator with the pullup of 2.2K. Functionality side we are not facing any issue. It is working fine. But in datasheet, it is mentioned as that this level translator will not support open drain and also pull value should be more than 50K. Is there any possibility of receiving failure in future with this level translator if we connected open drain pin in this level translator with the pullup of 2.2K. Kindy clarify.