Part Number: ADS127L18EVM-PDK
Other Parts Discussed in Thread: ADS127L18
Tool/software:
This is related to the same evaluation than in question https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1478299/ads127l18evm-pdk-an-issue-in-ads127l18-configuration-via-spi/5676049#5676049
Single channel works nicely with all tested sample rates 32Ksps - 512Ksps, but we have not been able to find a way to configure ADS127L18 to use two channels in time multiplexed mode with 64Ksps i.e. using only D0 data lane.
Expectation was to get samples from channel 0 and 1so that when there is no signal in channel 0, every second sample value is near zero and status byte carrying channel numbers 0,1,0,1...
Configuration below, can you find an error in it?
-----
retVal |= ratSpiWriteAds127Reg(GEN_CFG1, 0); // default
retVal |= ratSpiWriteAds127Reg(GEN_CFG2, 0b00000110); // fclk 32.768Hz instead of internal 25.6MHz
retVal |= ratSpiWriteAds127Reg(GEN_CFG3, 0b10000000); // full output slew rate in SAI, comment out for default slower one
// DP_CFG1 Texas suggested 0b01110000, difference in bits 5-4, which would mean 8 data lanes
retVal |= ratSpiWriteAds127Reg(DP_CFG1, 0b01000000); // data port status byte enabled, one data lane
// DP_CFG2 is mode depending
// CLK_CFG is mode depending
// GPIO registers are at default values (low disabled outputs)
// CHn_CFG1 default values (normal polarity, normal range, buffers disabled)
// CH0_CFG2 and CHN1_CFG2 is mode depending
retVal |= ratSpiWriteAds127Reg(CH2_CFG2, 0b00100000); // power down
retVal |= ratSpiWriteAds127Reg(CH3_CFG2, 0b00100000); // power down
retVal |= ratSpiWriteAds127Reg(CH4_CFG2, 0b00100000); // power down
retVal |= ratSpiWriteAds127Reg(CH5_CFG2, 0b00100000); // power down
retVal |= ratSpiWriteAds127Reg(CH6_CFG2, 0b00100000); // power down
retVal |= ratSpiWriteAds127Reg(CH7_CFG2, 0b00100000); // power down
// CHn offsets and gains at default values 0 offset 1.0 gain
switch(sampleRate) {
case 512: // 512Ksps, one channel
retVal |= ratSpiWriteAds127Reg(DP_CFG2, 0b00000000); // DCLK is 32.768
retVal |= ratSpiWriteAds127Reg(CLK_CFG, 0b00001000); // ext clock, div by 1
retVal |= ratSpiWriteAds127Reg(CH0_CFG2, 0b00000000); // OSR32
retVal |= ratSpiWriteAds127Reg(CH1_CFG2, 0b00100000); // power down, using only CHN0
break;
case 64:// 64Kbps, two channels
retVal |= ratSpiWriteAds127Reg(DP_CFG2, 0b00000000); // DCLK is 32.768
retVal |= ratSpiWriteAds127Reg(CLK_CFG, 0b00001011); // ext clock, div by 4
retVal |= ratSpiWriteAds127Reg(CH0_CFG2, 0b00000001); // OSR64
retVal |= ratSpiWriteAds127Reg(CH1_CFG2, 0b00000001); // OSR64
break;