This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80501: Requests for a Detailed Data of the Sink Current Capability (at Zero Code)

Part Number: DAC80501

Tool/software:

Hello.
This is Kwonjoon Lee from Samsung Display.

I would like to request a detailed data of the sink current capability in Figure 7-33, 7-34, and 7-35.

(Detailed Question)

1. What are the output voltages of the zero-coded DAC in the condition that the sink currents (from the Load to the DAC) are 0.15mA and 2mA, respectively.
    Please provide the above-mentioned output voltages of the DAC for the cases of Figure 7-33, 7-34, and 7-35.

Best regards,
Kwonjoon Lee