Part Number: ADS7852
Tool/software:
Hi, For ADS7852, what is clock min and max level, I am planning to to 8MHz TCXO, its max VOH is 2.6V. If i use this clock (VOH is 2.6), will the device work in properly?
Thanks,
RR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS7852
Tool/software:
Hi, For ADS7852, what is clock min and max level, I am planning to to 8MHz TCXO, its max VOH is 2.6V. If i use this clock (VOH is 2.6), will the device work in properly?
Thanks,
RR
Hi Rajashekhar,
Welcome to our e2e forum! The digital I/O levels listed in the table on page 3 of the ADS7852 datasheet show 3.0V as the minimum input high level, so the 2.6VOH of the TXCO may not work reliably. You need to be at least at the 3.0V level.
Hi Tom,
OK Understood, but as of now 8MHz TCXO's are not available with a supply voltage of +5V,.
Currently 3.3V TCXO's are available with an output voltage (VOH=0.8 x 3.3V= 2.64) So, can we use a Voltage Level Translator (TXB104) at the output of a TCXO to upconvert 2.64V to 5V?
Please suggest whether we can use a Voltage Level Translator for CLK voltage switching.
Regards,
RR.