This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S022: ADC SPI inconsistencies

Part Number: ADC128S022


Tool/software:

I have this ADC reading 8 analog inputs. The analog input is the same, but the data trasmited via SPI is not the same. 

This could be to irregularities in Analog Supply, Digital Supply, Ground Bounce? I have checked this three and they are consistent. 

Analog Supply and Digital Supply: 5V

Any tip?

Thanks in advance.

  • Hi Gabriel,

    Can you share the data that you are expecting, and the data that you are reading back? What input voltage are you giving to the analog input channels? If you have a logic analyzer available to probe the SPI lines, it would also be useful to check the output data you are getting.

    Regards,
    Joel