Other Parts Discussed in Thread: THS4541, , OPA320
Tool/software:
Looking at the ADS9227 datasheet, the application circuits in figs. 9.1, 9.4 and 9.7 all show the VCMOUT pin voltage being buffered though an unspecified op-amp, rather than being connected directly to the common mode input of the fully differential driver (THS4541). Two questions from this:
1. What benefit does the op-amp buffer give? I assume the VCMOUT voltage cannot drive much current but don't see any value listed in the datasheet.
2. If the buffer is needed, does it have any particular requirements? I assume VCMOUT is fairly steady and that something with low GBW would be OK but wondered if, perhaps, this pin sees any effects of sampling glitches. If I sample at 5MSPS, would you expect it to be safe enough to use something pretty basic with GBW of about 1MHz and decent noise spec, as long as it's unity gain stable?