Other Parts Discussed in Thread: ADS1115
Hi,
We are using an ADS1115 to read 4 single-ended channels using single-shot conversion mode. It works fine for a while, but after some time, we encounter an issue where the ADS1115 no longer provides correct readings.
This same issue occurs across multiple ADS1115 devices on different PCBs.
For example, I set a voltage of 3.6V using a variable power supply and measure the output using both a multimeter and the ADS1115. Initially, both readings are accurate. However, after about 10 minutes, the readings from the ADS1115 become incorrect.
issue -1. In one case, the multimeter still measures 3.6V, but the ADS1115 shows 6.143V.
issue -2. After 10 minutes, if I increase the power supply voltage from 3.6V to 4V, the multimeter correctly shows 4V, but the ADS1115 still shows 3.6V.
It appears that the ADS1115 is either hanging or freezing after running for some time.