Other Parts Discussed in Thread: , OPA561, OPA521, OPA541
Tool/software:
Hi All,
I am designing a programmable power supply using DAC81404. The datasheet (DACx1404 Quad, 16-Bit and 12-Bit, High-Voltage-Output DACs With Internal Reference datasheet (Rev. A)) has recommended the following circuitry for 200mA of output current.
Is there a recommended set of values/specs for the diodes, resistors and Transistors T1 & T2? If possible, can I get recommended part numbers for the Transistors.
Further, in the first page it is mentioned that using external circuitry we can achieve a high current drive of up to 1A. Can you point me towards any recommended resource for designing the current amplifier at the output of the DAC.
Thanks & Regards
Sudhir D