Part Number: AFE4460
Tool/software:
Hi TI team,
I’m working with the AFE4460 on a custom PCB and interfacing it with an STM32 microcontroller. I’ve verified that the SPI read/write functions are working correctly — I can read back register values. I’ve also checked the hardware connections multiple times and they all seem fine.
However, when I try to use the example code provided (specifically to power on the LED use the TXP pins), nothing happens — the LED stays off.
Best regards,
Jiajin Hou