Part Number: ADS7142
Tool/software:
Hi we are using the ADS7142 ADC for a new PCB.

We have just ordered some prototype boards and noticed that on the adress selector we have connected the voltage divider to DVDD instead of AVDD.
The DVDD is 3.3V and also the reference is 3.3V.
Is there a risk that the adress is not selected properly?
The resistors have 1% tolerance.
And DVDD is generated by TLV74133PDBVR.
So the DC accuary of the LDO should be smaller than +-1%.
Thanks in advance.