Part Number: AFE7950EVM
Other Parts Discussed in Thread: LMK04828
Tool/software:
Hello,
i need to change the configuration for this device but don't see a easy way to do it with the tools you provide.
I have access to all the docs and software via a colleague that have access to the repository in your website and I think I have everything.
I have a xilinx evm kcu105 and im using the reference designs for this board and follow the guide you provide to configure the boards and test the AFE7950EVM.
following the TI204c-setup.docx inside the repo
the only info i found for configuring the LMK04828 is in page 3:
after launch Latte. Run setup.py and devInit.py respectively.
- Configure LMK04828 clocking device on AFE EVM
Run TI_IP_10Gbps_8Lane_ConfigLmk.py.
I want to change the clocks used in the LMK04828 to achieve another sample rates.
so i need to configure the LMK04828 via this script
there is any place where is defined and explained the API used for this script?.
Regards.