This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5263 cheaper alternative

Other Parts Discussed in Thread: ADS5263, ADS62P42

Hello:  we have a customer looking for an ADC in the 40-100MHz range (TBD depending on implementation).  It is to be used as a CCD converter.  They are actively looking at the ADS5263 but it is very expensive,, so they are looking for either a different quad 14/16 ADC or a dual that they can use two of. 

The features that attracted them to the ADS5263 were:

-          Quad channel, but dual channel will work.

-          Dual 16/14 bit inputs per channel (only device I’ve seen it on). 

       Highest SNR possible

-          Decimation.

-          FIR filter (nice to have they are not sure if will be used or not).  Can you please recommend a quad or a dual ADC to meet this?  Thx.  EAU is 200 units / year. 

                     George Biner, Arrow LA FAE

.