Part Number: DAC8775
Tool/software:
TI,
I am currently testing the 8775EVM board, and everything appears to be working as intended. I plan to use three of the four channels strictly for 0–20 mA output. I would like to utilize the full input voltage range of the DAC (12–36 V). If I do not use the negative power supply on any of the channels, plan to use the buck-boost feature with full tracking, and do not intend to use the fourth channel, what simplifications can I make to the reference design? Am I able to eliminate some of the external components? With the exception of the inductor, can I eliminate all of the components in the red rectangle and tie LP_A and VNEG_IN_A to ground? I would assume that there aren't any components that I can remove on the output side?

Thanks,
Jason