Part Number: ADS131M02
Other Parts Discussed in Thread: ADS131A02
Tool/software:
Hi all,
Recently, I designed a simple SDR that uses some low-noise audio op-amps to amplify the weak down-converted signals and sample the IQ paths by a single ADS131M02.
The challenge I am now facing is the unmatched common-mode bias using a simple-ended power supply: the low-noise op-amps are bipolar devices and have output ranges from AGND + 0.6 to AVDD - 0.6, while ADS131M02 recommends the input to any AINx pins to be AGND - 1.3 ~ AVDD - 1.8 for gain >= 8. When AVDD = 3.3, setting a DC bias that satisfies the dynamic ranges of both devices at any gain is difficult.
Thus, I'm thinking if it is a good practice to use AC coupling between them. I found several notes (see below for an example) mentioning this technique, and it seems like it is likely to work for ADS131M02 too.

I also noticed that in ADS131M02's datasheet, there's a demonstration of measuring the current, where the common mode bias is set to AGND and the signal path is somewhat similar to AC coupling (by a transformer).

My questions are:
1. Can I use AC coupling in my design like what the first figure shows?
2. Can I simply set the Vcm = 0 (AGND) like what the second figure shows? As the ADC can only measure differential signal no higher than +-1.2v, I think this won't cause any trouble even at the lowest gain?
3. Should I tune the parameters of the anti-aliasing filter after AC coupling?

4. Any other tips or cautions when selecting the components' values? I saw something called pop noise from larger coupling caps, but I don't think it is as serious as I'm not going to read the results immediately.
Any help would be appreciated. Thanks in advance.